Hello,
I am trying to understand how the Soft over current limiting works on the UCC28180. I am building a 3kW PFC but the I_SOCcurrent is limited to 30A at the moment.
When I apply an overload at the output, I see that the PFC current starts to lose control and you can see the bump in the waveform below. This is also seen in simulation. I would have expect it to start clipping at the point of the Soft over current limit. Could anyone explain why this happens and how I can control it.
CH1: VIN CH2:I_IN, CH3: V_boost, MATH: P_IN
Applied load: 35 Ohms
Thank you.
Regards,
Pravin