Hi, all.
I have a problem about my SMPS circuit with the UCC28630 that no voltage appears at secondary side of transformer.
I've checked the circuit, and found no voltage appears as well at all pins of the UCC28630 except for the HV pin at which I can see around 16.5V. I've tried to debug where this failure comes from, but failed. Could you let me know if you have any good idea to solve this problem?
For your reference,
- I used the WEBENCH design tool to design the SMPS, and the attached diagram is the one I got from the tool. I've made my SMPS circuit exactly same as this diagram.
- I've also checked the power transistor, M1 separately, and it's OK. It works and was destroyed.
- There was a sequence of events to failure.
- At first, as we saw no voltage appears at the secondary side of the transformer, we found D1 was mounted reversely. Then we corrected it, however the SMPS still doesn't work. I'm not sure if this incorrect mounting of D1 could permanently damage on some components in the circuits.
- second, after repairing D1 position, we found also a surface of the transformer was melted partially as you can see in attached picture, so I wonder where this comes from, and if it could be an symptom of the failure.
Thanks in advance!!