Hello everyone,
I design an EMI filter to which 3 identical DC-DC converters are connected in parallel and I want to ask you how to calculate output impedance of EMI filter for this case?
P.s. Each of DC-DC converter's have internal LC-filter.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
I design an EMI filter to which 3 identical DC-DC converters are connected in parallel and I want to ask you how to calculate output impedance of EMI filter for this case?
P.s. Each of DC-DC converter's have internal LC-filter.
Hello Constantine,
This is a good question.
Here is a good paper that sums it up.
www.ti.com/lit/an/snva538/snva538.pdf
The filter output impedance will be the same no matter how many converters are connected to it.
Each converter will typically have a NEGATIVE input impedance, and impedances in parallel will act like resistors in parallel.
The main goal is to make sure the EMI filter output impedance is much less than the summed converter impedance.
See figure 3 in SNVA538.
Each filter upstream must have lower output impedance than what is connected to it.
So the Main filter must have lower output impedance than the summed input impedance of the DCDC's internal filter.
You must be able to quantify the DCDC internal filter details.
It is probably best to model the filter as above so you can see the impedance vs frequency curve.
You can use TI-TINA spice based simulation program to model this.
Thanks for paper's!
Maybe I'm wrong, but the internal filter is the last stage of the emi filter, and in the case of three dc-dc converters with parallel connection, we have the last stage of the emi filter, which consists of three parallel LC filters, right?