Are there any Buck regulators available which have watchdog reset function inbuilt? Below are the parameters for buck-
VIN= 9V to 24V, Vout=5V, Iout=3A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are there any Buck regulators available which have watchdog reset function inbuilt? Below are the parameters for buck-
VIN= 9V to 24V, Vout=5V, Iout=3A
Hi Priyanka,
Let's me confirm the purpose of that watchdog timer first, what's function do you want to get from it? Maybe we have that function built in our part but not called watchdog. And what's the application of your product, any special requirements?
BRs,
Ryan
Hi Ryan,
Thanks for the response. Watchdog means it will take one PWM input(continuously) from microcontroller. Its output is connected to reset pin of microcontroller. So, it will reset the MCU in case of no PWM(watchdog signal) input from MCU
Hi Priyanka,
So you want a DCDC with watchdog built in which could communicate with an external MCU, right? To make the DCDC more reliable or the MCU?
For a more reliable DCDC, some DCDC part has a "Powergood" function, like LM43603-Q1. But few parts with powergood function could meet the input voltage rate as well as the output current rate.
Ryan
Hi Priyanka,
Thanks for your info, sorry, I didn't find such a part could meet your requirements in our product line. it's an special application. So there is no WATCHDOG timer built in the MCU and you want to find a buck regulator with the WATCHDOG timer built in. I suggest to use an additional external WATCHDOG timer to meet the application, like TPS3851. What's your comment about it?
Ryan