Other Parts Discussed in Thread: UCC28180
UCC28056 Can Cover Vin AC 90-264V 50~60Hz and 400Hz application?
Po under 150W,
Vout DC 15V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yunsheng,
May I know when can the team come out the answer for 400Hz input support? If UCC28056 not works any alternative solution?
We need to final the solution recently.
Thanks!
PY Tsai
Hi, PY
UCC28056 does not fit for 400Hz because of internal circuit limitation.
what is the power level you want to design? UCC28180 can support 400Hz input voltage, also can support 50/60Hz input.
Regards,
Yunsheng
Hello James,
I am attaching test data that was taken on the UCC28180 EVM.
There is three pages to the document
Page 1 is the data at 50Hz and 60Hz
Page 2 is the data at 360Hz
Page 3 is the data at 800Hz
If you hover the pointer over the line current column you can see what the scope waveform looks like.
In most cases the power factor is greater than 0.9
Regards
John