We'd like to use the UCC28950 full-bridge controller to design a DCDC converter with input voltage between 45V and 130V, and an output voltage of 350V.
The output power is 2200W. Is it suitable for this type of applications?
We have tried to use it but we are having a lot of problems to stabilize the control loop (we have followed the recommendations given in the reference design SLUA560B).
The only difference with the reference design (in addition to the input and output voltage ranges, and the output power) is that the current sensing (CS) is done with a sense resistor on the bottom NMOS SOURCE.
Regards.