My customer is using the UC3525 and is noticing a fair amount of variation of dead time with temp. They have the following questions:
1. Is deadtime controlled or characterized in any way? I see a curve in section 6.6 (above) but no measured specs in section 6.5 for deadtime.
2. Is the correlation between dead time and temp (higher temp is more dead time) a known and “correct” behavior?
3. Our design uses 470pF for CT. Section 6.3 recommends only down to 1000pF (twice our value), but the Maximum Frequency parameter in section 6.5 uses 470pF so it makes me think this may be fine.
Thanks,
Dan