Other Parts Discussed in Thread: UCC27531, UC3708
HI Sir
May I know TI have VDD > 25V dual gate driver solution like UCC27324?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kai,
I am an application engineer at TI supporting low side drivers and will address your question. TI does offer a dual driver with up to 35V operation which is the UC3708. This is an older bipolar device however, so you may want to consider the UCC27531 which is a single driver available in a compact SOT-23 package which has a 35V VDD rating.
Please confirm if this answers your questions.
Regards
Richard Herring