Hello,
Do we have a solutions for the requirements below? any reference designs?
380VAC – 480VAC 3phase coming in. Rectifier then creating 500-700V DC bus
Regards,
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello David,
I think you are asking for a pfc type power supply that can operate from a rectified 3 phase source.
Is that correct?
There must be some more design requirements such as power levels,efficiency,power factor, cost .... etc etc.
Do you know what the application is ?
Any of the pfc controllers can be used to generate 700V DC from a rectified 3 phase 480Vac
In high power application you can use the UCC28180, UCC28070 or the UCC2817A
The reference designs for these parts are all for single phase 85Vac to 264Vac with a 400Vdc output
It is a straight forward task of changing the rectifier from a single phase to a 3 phase and setting the output voltage to 700Vdc
Regards
John