Other Parts Discussed in Thread: UCC28740,
Hi,
According to the datasheet of UCC28740 (e.g. page 10), the required "turnon UVLO" voltage to start the chip is 21V. But in the schematic of PMP11451 the VDD of UCC28740 is only 17.3V:
The voltage from the auxiliary transformer output is at first rectified (D9, C100) and then regulated to 17.3V by selfmade LDO (Q1, D10). 18V - V_BE = 17.3V.
So 17.3V is less than 21V and thus not enough to start up the device.
Am I wrong?
Thx
Daniel