Hi,
I am working on a PFC stage using the UCC28180 as shown in the schematic but the IC does not startup...Any suggestions on what I am missing?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am working on a PFC stage using the UCC28180 as shown in the schematic but the IC does not startup...Any suggestions on what I am missing?
Thanks
Hello Ioannis Manousakas,
You need a voltage of greater than 12V on J2 and a voltage of greater than 65V on J1 in order to get a gate drive signal to the MOSFET.
Please make sure these voltages are present and that the circuit is wired as in the schematic
Regards
John
Hi John,
Thanks for the information. I managed to better understand the controller start up!
The bus capacitance is actually the C16=680uF.
The controller needs the VSENSE and VCC as you mentioned and sometimes a small negative voltage at ISENSE for startup.
I managed to have gate signal but only without the Vin... When the Vin was increased VSENSE increased and the controller started momentarily. Probable because the layout was not done as suggested in the datasheet, the controller was damaged...I will modify the layout and test it again.
Thanks again for the help.
Regards,
Ioannis