Dear,
I have one non-isolated DC/DC project which needs to choose the proper controller IC. The spec. is:Input:18~36V,Ouput:15V/45A. So the topology could be single BUCK or two phase interleaved BUCK. From the thermal consideration, two phase BUCK may be more suitable. I don't know whether two phase BUCK using two independent IC or one IC which has two phase function is better? Could you please recommend the proper IC or solutions from your side. Here the foot package of TSSOP is prefer.
In additon, i have one question to the BUCK IC definiton of Iout(max). Is the value of Iout(max) determined by the external Mosfet driver loss? Can we choose the smaller Iout(max) if we use external driver circuit? Does it mean the output current must be smaller than the Iout(max) defined in the quick search website. Can we use two IC which Iout(max) is 20A or one IC which Iout(max) is 40A for the application of 45A of output current in our spec.?
Look forward to your reply. Thank you very muck.