hello
In SLUSA16D, in design and implementation, why RC snubers are not used for power MOSFETS ?, how turn off snubbing is achieved?
thanks
samrat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello
In SLUSA16D, in design and implementation, why RC snubers are not used for power MOSFETS ?, how turn off snubbing is achieved?
thanks
samrat
Hi Samrat
The PSFB is a zero voltage switched topology and doesn't normally need snubbers on the primary. When the 'bottom' switch turns off, the voltage swings positive where it is clamped as the body diode of the 'top' MOSFET turns on. When the top switch turns off then the voltage is clamped by the body diode of the bottom MOSFET - snubbers are not needed because there is no unclamped inductance available to generate the large spikes. This is in contrast to the Flyback topology for example where the leakage inductance energy has to be absorbed by a snubber in order to prevent it generating high voltage spikes.
Having said that - the assumption here is that there is no unclamped inductive energy in the H bridge. This is true if the PCB layout is good but any stray inductance in the source or drain circuits of the MOSFETs will generate spikes - the solution is normally to improve the PCB layout but a snubber would also work.
Hope this makes sense.
Regards
Colin