Other Parts Discussed in Thread: UCC27324
Hi Sir
Would like to use UCC27324 or UCC27524 to replace NCP81071
May I know what's the benefit of UCC27324 and UCC27524 ,which one you suggest to use
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
Thanks for asking about this question. Im an apps engineer and will help to answer it. UCC27524 is the best replacement part for NCP81071. The UCC27524 has the added benefit of half the prop delay, one tenth lower quiescent power consumption and half the operating current across frequency. UCC27524 has less variation in rise and fall times across temperature, we also show thresholds and output resistance across temperature which show a flat curve and lower output resistance. Most importantly UCC27524 delivers its 5A peak current during the miller plateau, when it is needed most. This makes UCC27524 capable of sourcing high current at low voltages.
Does this clear up the benefits. If you need further explanation please tell me how you plan on using UCC27524 and in what application?
Thanks,