I am working with the Mathcad worksheet for this part from sluc644. In the "Neutron..." worksheet I don't understand the calculation for VCST_OPP(Vin).
The graph for VCST_OPP(Vin) looks like it is meant to duplicate Fig 34 in the IC data sheet, but with Vin as the x axis rather than IVSL. Is that correct?
Trying to correlate the two, I don't understand the formula for Vin_IVSL(Vin). Does this function calculate the voltage on the VS pin as a function of Vin? If so, shouldn't the resistor values Rvs1 and Rvs2 and the Naux transformer winding ratio be part of that? What does the fixed 106 V in the function represent?
And I don't understand the fixed voltages in the piecewise function for VCST_OPP(Vin). It seems like they are intended to create the breakpoints in the OPP curve like Fig 34, but since Fig 34 is a function of IVSL shouldn't the breakpoints depend on at least Rvs1 and Rvs2? Maybe that would be taken care of if Vin_IVSL(Vin) depended on Rvs1 and Rvs2?
Thanks for any help.