Hi Sir
May you pls help double check our application circuit?(5Vin /5Vout/0.3A lout)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
May you pls help double check our application circuit?(5Vin /5Vout/0.3A lout)
Hi Bogey,
I put the component values into the excel calc tool and the file is attached below. The main finding I have is the compensation looks like it has too much gain. I suggest reducing R619 to ~12.4 kΩ.
I see the fsw was increased to 650 kHz. Any particular reason for this? If you'd like to get better effiicency you should be able to decrease the fsw to as low as 300 kHz without any issues. The biggest trade-off would be slower transient response.
Can you share some details on the application?
Thanks,
Anthony