This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eddie,
Thanks for your interest in UCC27714! I'm glad to see your project is close to completion.
Eddie Loy said:QUESTION 1 : STARTING WITH THE KNOWN PARAMETERS LISTED ABOVE, ARE THEY GOOD NUMBERS? FROM WHAT I GATHERED FROM THE DATASHEET THEY AREREALLY CLOSE.
The HB-HS voltage drops from 16.4V to 12.4V, considerably lower than normal for driving IGBTs (typically we see at least 15V at all times). The gate charge of the selected IGBT is less than 100nC, and since C = Q/V, this suggests the value of the bootstrap capacitor is smaller than expected (around 0.025µF, vs 0.1µF in the schematic diagram). What is the construction and voltage rating of the nominal 0.1µF bootstrap capacitor? For example, a small 0603 ceramic capacitor with 25V rated voltage? The total capacitance of SMT capacitors can shrink with applied voltage, for example see this Murata FAQ.
Please try replacing this capacitor with a larger value and check if Q1 is fully turning on in that configuration.
I believe the above answer should cover question 2 as well.
Eddie Loy said:QUESTION 3 -- DO YOU HAVE ANY ADVICE, SUGGESTIONS, POSSIBLE SOLLUTIONS THAT WILL HELP ME FINIS PROJECT?
First, I believe that placing FQPF13N06L as SH is not sufficient. Since the HV source is 60V, the IGBT will be operating very close to breakdown, and any noise or ringing on the switch node could damage the circuit. I recommend a component with breakdown voltage greater than or equal to 100V for SH.
I also recommend selecting transistors which are optimized for lower current and lower gate charge, to decrease the gate capacitance and allow for rapid turn-on even with a large gate resistor. SH requires a higher voltage since it is placed directly on the HV source, but SL operates only up to 18V and could possibly be replaced with a smaller, less costly component.
If the input capacitance of SH can be reduced to 500pF or less, you may find it advantageous to connect SL drain to SH gate directly, and to increase the value of RSHG to 1kΩ or more. Since the duty cycle is less than 50% at 100kHz, the charge path for the bootstrap capacitor through SH should have at least 5µs to activate during normal operation, so as long as the time constant of the input capacitance and gate resistance is kept small relative to this 5µs off time, the recharge circuit should behave equivalently. This will also substantially reduce your power supply current requirements, since you will no longer be shorting the 18V supply to ground through 13Ω every cycle. SH will also be clamped off very quickly by connecting SL drain to SH gate directly, preventing a shoot-through path from forming through Q1 and SH.
Regards,
Hi Eddie,
Most of the changes look reasonable. A few things stood out:
Best of luck with the design.
Regards,