Sometimes when using this part, I notice The signal in is 1/2 the voltage, and the output is half.
i.e. Vin = 3.3, VDD = 5. However, When using a multimeter on the chip I'll see Vin = 1.7, and the output will be 2.5V instead of 5.
Any idea what is causing this? Both EN pins are left floating.