Hello
Do we have solution to meet below customer requirement? Thank you.
AC/DC
--Isolator/Non-Isolator
--input: 90V to 265V (AC)
--Out: 5V/0.6A (DC)
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Patrick,
Thanks for your interest in TI. An AC/DC flyback should be able to meet your power requirements. PMP8757 is a reference design that may be of interest to you. This is a 90Vac - 264Vac to 5V output @ 1A max using UCC28700.
Best Regards,
Ben Lough