Dear Sir,
I am designing dual Vout (Vpos and Vneg) using TPS65131.
The desig requires to vary each Vout voltage range as follows;
VPOS : 3V to 15V
VNEG: 0V to -15V
controoled by DAC analog outout (use AMC7812B).
The method is to feed current and connect the DAC outs to FBP and FBN pins through resistance (named RDAC0/RDAC1). I am attaching an simple block diagaram and calculations.
AMC7812B DAC output will have 0 to 5V full scale voltage swing range.
7142.TPS65131 Unveral Vout.pdf
May I get your review if this will work?
I would appreciate for your advaice.
Best regards,
Masa