Hi,
Now need OLED power spec as below
Input Voltage is 12V or 24V
Output Voltage is below for checking again.
1. 1.65V~4V/1A for 2 Channel, Ripple <1%
2. 1.65~10V/0.5A for 2 Channel, Ripple <1%
3. 1.65~8V/2.5A for 1 Channel, Ripple <0.7%
4. -8V~ -1.65V/1.5A for 1 Channel, Ripple <1%
5. 6~9V/0.5A for 1 Channel, Ripple <1%
Please kindly help to suggestion solution for reference.
Thanks.
Regards,
Eric