Other Parts Discussed in Thread: TPS65165
Hello,
while comparing the functional block diagram (Figure 20. of the TPS65165 datasheet of Feb 2017) with the reference design of the TPS65165EVM in slvu548 I noticed that in the datasheet the diodes connecting to VN and VB_SW seem to be Schottky diodes. Also Table 21 of the datasheet, section 9.2.2, two Schottky diodes are listed (BAS3010, MBR130T1). In the reference design of the TPS65165EVM all diodes are Schottky diodes MBR1301T. In my design I am using all BAS3010, and that doesn't seem to be working. Is it critical to have the MBR1301T diodes to VN and VB_SW?
More precisely, are Table 21 and Figure 20 to be understood in the sense that the diodes to VN and VB_SW should be one of the Schottky diodes (BAS3010, MBR130T1) and all other diodes (at or near VDDH_D and VEE_D) may be any of the three, i.e. either Schottky or the non-Schottky BAV99?
Thanks,
Markus