My Circuit is shown below. My AVDD or Vo1 is outputting slightly lower than the computed value. My target is 9.6V but I am only outputing 9.12-9.14V. My LCD requires 9.4V-9.8V for this. Since my AVDD is slightly off, my VCOM also is off with output of 3.85V instead of 4.09. The VGH(Vo3) and VGL(Vo2) is fine and are just in 20-60mV off which is fine for my application. I checked my resistors for the first output and they are correct (62k and 430K). To produce 9.12V, my R2 should be around 65K(I don't have this value or anything near this value aside from 62K). I did not attach load. Is the output affected by load?