So I've been working on this IC for far too long. I'm making a development board for a 5" TFT LCD.
The IC starts up and the 5v buck regulator starts just fine, but VGL only goes to -5v. It then faults out if I have faulting enabled since it never reaches the full -10v. This prevents VGH and Vcom from ever starting as well. I can disable the fault by removing C8 in the schematic below, which I've done, but then VGL just stays at -5v.
So somehow the IC knows that it's not at the full -10v but the system isn't responding. I've gone through two pcbs with the layout, the first was a 2 layer which wasn't laid out very well. The second is a 4 layer with a much better layout but the behavior is the same. I even checked every single component when I made the 4 layer board to ensure I had no faulty parts. I've also tried multiple TPS65150 IC's
I've included my full schematic below and the only difference is C8 was jumped and is no longer there disabling the fault, and I'm using a 2.2uF cap wherever it says 4.7uF. The power requirements are only 20mA for the 5v buck, and 250uA for the -10v line and +15v lines. I also attached some external resistors to simulate the loads so the charge pumps will operate. Is there anything wrong with my schematic? I'm really at the end of my rope with all of the debugging. I'll try to upload a snapshot of the power on sequence later.