Hi,
I'm using the TPS65185 on my board.
This board is from my own design, and the magnetic noise is too high.
I quickly compared to a KOBO board, which also have a TPS65185, and the magnetic noise is significantly lower than on my own board.
Questions are :
1. Is there any adjustment that can be done on TPS65185 registers that can reduce the magnetic noise ?
2. It seems the noise mostly comes from the inductors. I used the recommended NR4012T2R2M and LQH44PN4R7MP0, which are said "shielded". Kobo's coils seems smaller, may they be the most significant source of noise reduction ?
Thanks for help !
Best regards,
Vincent.