This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65100-Q1: Schematics Review Needs

Part Number: TPS65100-Q1

7558.217EA01_ TPS65100-Q1.pdf

In  Fig.3 of TPS65100Q1 datasheet page 13:

a.W/o 3.3V output needs, is it ok to treat ENR & FB4  pin as  NC?  BASE pin connected to VIN is ok ?

b.is below design OK?  

                       R1=806K,R2=75K ,C5=3.3pF for VDDA

                       R5=1M,R6=45.3K for VGH

                       R3=750K,R4=150K for VGL

c. is it ok if COMP pin adopts R(4.32K)+C(2.2nF)?