I have a quesiton.
【Question】
An unexpected rewrite of data occurs in an external flash ROM.
What kind of problems will occur if "1" is written to "D14" "D11" of DAC MSBbyte (49h)?
【Actual Behavior】
· The "D11 = 1" setting seems to have no problem, outputting the target voltage.
· Behavior due to "D14 = 1" setting is unknown (appears to be working normally).
However, since it is stated that "0" is set on Datasheet, we want to check the influence due to SPEC violation status.
Best regards,
Ozawa