This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM36274: Looking for a power supply o support LCD bias and WLED backlight

Part Number: LM36274

Hi,

 

I’m looking for a DC-DC boost converter for TFT LCD bias and backlight. Input is +12V or +5V, output is +24(5mA), -6V(5mA) for LCD bias and 21V(200mA) for backlight.

I see TI has such part, such as LM36274, but its output is +/-4V ~ +/-6.5V for LCD bias.


Can you please recommend a part for my application?

 

Thanks.

  • Hi,

    TI does not have a single device that fits your design requirements. Are you open to a 2-device solution?
    Also, could you specify how many backlight channels are required?

    Regards,
    Angelos Tsiros
  • In reply to Angelos Tsiros:

    Hi angelos,

    Thanks for the reply.
    If no specific part fits my requirement, I am okay to a 2-device solution. One is dedicated for LCD backlight. The backlight ciruit is 7LEDs in series, typical LED forward voltage is 3V. Do you have any recommendation?

    Thanks,
    Carrie
  • In reply to Caiyun Fang:

    Hi,

    You can try the TPS61500 for backlight and the TPS65100 for LCD bias. If those are not exactly what you need I would recommend starting new E2E threads under those devices because the teams supporting those products would be better equipped to help you further with this.

    Regards,
    Angelos Tsiros

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.