Hello,
where can I download the LP5521x4easy.exe mentioned in http://www.ti.com/lit/an/snva241c/snva241c.pdf ?
I don't have a kit, but I would like to use the command compiler.
Regards,
Lo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lo,
I can help you with that. Please send me an email and I will help you to get the program.
-Sami
Hi,
This program should be included in the evalution kit. If it is missing, please contact your nearest sales office.
Thank you,
Sami
Hi Sami,
I don't have the evaluation kit, but am planning on using the device in a product. Is it still possible to obtain the program?
Thanks.
Regards,
Tim
Hi Tim,
I am not sure how the evaluation SW would help you without the evaluation board. They are meant to be used together.
If you are looking for examples there exists the linux drivers for LP5521.
Thank you,
Sami
Hi Sami,
I was hoping to use the software to generate numerous programs as hex files that can be stored in embedded memory and retrieved and sent to the LP5521 during operation.
Regards,
Tim
Hi Tim,
The evaluation program does not contain the compiler, which generates the hex-codes, so you would need to obtain that instead of evaluation SW. You could contact your local sales office for that.
Other option is to use the LP5562 compiler. It can be downloaded from the LP5562 folder (Tools and Software). The devices command execution engines are the same and you should be able to produce workable hex-code with LP5562 compiler also for LP5521.
Regards,
Sami