Dear team,
A customer wants to customize the design on LM3414HV. The purpose is to eliminate the bias current. Could you please help?
- is it possible to insert an switch between Vin track and pin 8 Vin?
- And in general, is it possible to use different voltages for the Vin pin? Example: +12V on the Vin but +24V in the Vin net?
- is it possible that do not connect Vin pin and supply 5V in the pin1 (VCC)?
The purpose is to eliminate the bias current when the LM3414 is not in working, but if possible even when it is working. Can you please advise?
Many thanks!
Xun