Hello, I'm not clear this is the optimal place for this error report but there seems to be an error in the timing chart for this 16-channel LED shift register, datasheet located at http://www.ti.com/lit/ds/slvs677/slvs677.pdf
On page 4, the timing chart indicates output pins 0,2,5,10,11,12, and 15 should be sinking current -- according to SDI. However, it is unclear whether the data is inverted as output pins 4 through 14 are excluded, and both sides are identical from the reader's perspective. If it is assumed the data from SDI on clock signal 1 corresponds to OUT1, then OUT2 and OUT3 should be inverted.
This is in need of correction very soon.