Hello,
I want to use the EN pin on the LM3409 to turn ON and OFF the driver (LED's).
I will use a toggle switch to connect the EN pin to GND for OFF condition and for ON condition the switch is open and EN will be pulled up with a 10kOhms resistor to VIN.
VIN 8-18V.
Is that ok? Is 10kOhms ok?
I will have 4 identical drivers on one PCB, same VIN and GND. Is that ok? Something to think about?