Hi,
I want to design an LED driver using UCC28810 with following specs
Input = 90V to 270VAC and
Output = 65V at 1.15 Ampere - constant current
Kindly suggest the transformer details.
I have a few questions :-
a) Is UCC28810 the best suitable LED driver for this requirement (where PFC is NOT a must , but if available, it is ok !!)
b) Is there a design tool to generate the transformer details using UCC28810 ? (I could NOT find the same on T I website)
c) What is the frequency of operation of this device ? I could NOT find it in the data sheet
Regards
Atul Bhakay