Referring to the CSH pin on the LM3429, I want to overdrive it with 2V or so (its rated to 6V ABS
MAX)to turn the LED drive off. It looks like that will shut down the PWM
I just want to confirm that and that there won’t be any issues.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Referring to the CSH pin on the LM3429, I want to overdrive it with 2V or so (its rated to 6V ABS
MAX)to turn the LED drive off. It looks like that will shut down the PWM
I just want to confirm that and that there won’t be any issues.
Hi Andy,
The biggest concern is the leakage into the CSH pin:
Please look at how much current is sourced into this pin when over-driving it.
A better way might be to simply drive nDIM to GND. When not in PWM mode, this is basically a UVLO pin. So grounding it should disabled the part.
Let me know what you think.
Regards,
Hi John,
Tell them the same thing I'm going to tell you. It is a simple question. Know when to pick your battles and answer it. If you guys are truely intrigued with the application and design details, I will set up a call with the designer to review it in detail with you in detail... Provided you come prepared with some answers.
Thanks, Andy