Dear All,
I am trying LP5521 LED driver, there is no any problem on DIRECT mode, and load flash pattern one time then execute.
but if I am trying to load different patterns and run. It will be very unstable.
Repeat loading/execute seems to easy be fail. Sometimes it can display right pattern, sometimes go bad, or display a strange pattern.
Does loading just can do only one time after power on?
(commands pattern has no problem, and have enough wait delay for OP_MODE/ENABLE registers writing)
Already try many ways but can't find a rule.
Does any one have same experience? Thanks very much.
p.s. I've seen a code on the WEB shows below, is there any problem on IC?
/* 299 * Make sure that the chip is reset by reading back the r channel 300 * current reg. This is dummy read is required on some platforms - 301 * otherwise further access to the R G B channels in the 302 * LP5521_REG_ENABLE register will not have any effect - strange!