Hi there,
I am working on a 0-10V dimming solution based on LM3414 to drive a LED string. I understand that I should use the DIM pin of LM3414 for dimming the LED string. Unfortunately there did not exist an UL approved 0-10V dimming driver for this kind of application. Nevertheless I did an experiment by hooking a 0-10V constant voltage dimming driver to the LM3414 without connecting to the DIM pin. The output of 0-10V dimming driver feeds a 24V PWM signal to the Pin 8 (VIN) of LM3414. I found that the LED string could be dimmed by varying the control voltage of 0-10V wall box dimmer switch without flickering. Is it OK to feed this 24V PWM dimming signal directly to the Pin 8 (VIN) of LM3414 for extended period of time without damaging the IC?
Cheers,
Bill