Hello We are using the LM3429 Chip
Vin 10.3 min 28 Vin max
V outmax =40V I out =2.1Amps
When we tested the unit we receive a screech from the inductor, looking at the waveform, the inductor is bouncing from discontinuous to continuous conduction mode. Looking at the Drain wave form the voltage indicates that the duty cycle is changing for no reason ( no Vin change) When this occurs it discharges the inductor and so it goes DCM and then tries CCM for little bit.
Since we are using analog dimming we have 1uF on the compensation Capacitor,
1 K ohm for each of the RHSN and RHSP, RCHS is 12.4K , Cin is 20uF and Cout is 20uF. We have tried with 5uH 10uH and 20uH inductors.
Another effect that is seen is that during a particular voltage say 16V , the output stabilizes but outputs far more current than the calculation says should be possible, to ensure that this was not an effect of the trace resistance various resistors R150 R130 R100 have been used but both overshoot the 2.1Amp limit ( This should take a resistor of 0.047). If we exceed 20V , then the current drops to 600mA total, but is stable again but in DCM. Using Webench we matched exactly what we had in our circuit and we still get the same results.
Thank you for your assistance.