Hello,
i don't see the maximum ground current rating through the ground pin (pin 4) for the TLC5973. Can all 3 outputs run at 50mA simultaneously along with 10mA of Icc current. If so, max total would be around 160mA based on shunt regulator usage. However, this isn't specified in the datasheet. Any help would be great.
Thank you