The LM3499 Demo board is five channels, each set to 0.35 amps.
If I connect three LED strings (leave two channels open), will the three strings current regulate to 0.35 amps each (1.05 amps total)?
Or, will the board try to regulate to the total of 5 x 0.35A = 1.75 amps? [1.75/3 = 0.58 amps per string]
If the answer is 1.75 amps, how do I turn-off the two unused channels?