Hello All,
I am working on a buck-boost design with the LM3429, for which I have some questions.
The design will have specifications:
input voltage: 20-28V
Output voltage: 20V
Output current: 5A
The LEDs will be connected between Vin and Vout (so not ground referenced). That means that the boost output voltage can be up to 48V.
Question 1:
Is it feasible design the supply on IMS? The metal substrate will only allow me to use one layer. That means that I cannot use a ground plane below the circuit or cross tracks by using other layers.
Now if I need to make a few crossings I can still use 0R resistors as bridges. But it cannot be too many. Another concern is EMC. I do have a large chunk of aluminimium below the circuit, but I can only bind this to a potential by grounding the whole housing. Also Aluminium probably does not conduct as well as copper. As the switching frequency is around 500Khz and the switch node voltage will have a delta of up to 48V I am not sure if emission can be within limits.
Question 2:
would it be wise to choose a 1206 package for RCS? The average power dissipation would be about 350mw, so the dissipation is not a problem, but the peak switch current will be 11A. This means that the current density will be rather large and the pad sizes are relatively small. On the other hand if I would use a 2512 package the loop may be larger. In any case it would use more area.
Thanks in advance for your help.
Ronald