I'm looking for a simple circuit to drive strings of LEDs that require 160v @ 100ma. The TPS92410 looks ideal but I'm wondering if the TPS92411 drivers could be omitted and just have the TPS92410 drive the entire string? The LEDs are part of an assembly and it would be difficult to tap into the middle of it to use the TPS92411s.
Or is there a better solution with low component counts and inductorless?
Thanks!