Hi Team,
I understood TPS61169 features a thermal foldback function.
Is this protection auto recovery?
(Does the current limit value increase to normal one if the junction temparature decreases from 100℃?)
>When the junction temperature is higher than 100°C, the switch current limit ILIM is reduced automatically as Figure 2 shows.
I would also like to know the value of current limit of Ta>100℃. I couldn't catch the value in Figure2.
Best Regards,
Yaita / Japan disty