I am evaluating the TPS92640 for use in a low output voltage current source application. The parametric data for the TPS92640 states that Vout min is 0V, however the datasheet leads me to believe that the Vout pin expects to see a scaled down version of the output voltage centered at 2.5V. This would imply that the minimum output voltage is 2.5V.
Can anyone answer this?