Hello,
we are using designing with the TLC5973, and the chart below from the data sheet suggests that there is a dropout voltage or an overhead at the driver output to maintain constant current regulation. It looks like it is about 300mV at 10mA. Can you confirm required voltage at 5mA, 10mA and 20mA?
Thank you