Hi.
I'm using the LM3409HV evaluation board straight out the box.
The graphs in the LM3409 data sheet (figure 17) and the AN-1953 LM3409HV Evaluation Board User's manual (Figure 6- and Figure 7) showing LED current vs EN pin waveforms show the LED current falls to 0 in about 2 or 3 us max after the EN pin goes low.
On my scope I'm seeing a first order decay which takes about 100us to reach zero! (Time constant to decay 66% about 20us maybe)
Why the huge difference?
I have all the standard component values on the board - I have not modified the eval board in any way.
J1 is not fitted at all so it's in EN pin PWM control which I'm drive with a clean 3v3 waveform from a sig gen reference to the eval boards gnd.
I have limited Iadj with a fixed resistor divider external to limit LED current which works fine - this is fixed throughout test and does not vary though I have tried values from 100 to 500mA but doesn't affect time constant of LED decay current .
I'm observing the decay on the LED +ve drive o/p voltage and also by putting very small (0.1ohm) high side sense resistor in line + amplifier to measure the actual current waveform.
I have 12 LEDs with Vfwd about 3.3V at 350mA.
The input voltage to the LM3409 is 48V.
I was wondering if this could be the main inductor time constant but it's the one on the eval board that presumably that the waveforms were taken with. Why do I see such a long decay compared to the graphs?
I need fast decay time for the application in question. I also need very high efficiency so ideally don't want to use the shunt method.
Thanks,
Chris