I am using a TPS92512 operating from a rectified DC power supply. The circuit is based on the reference design, operating at 1A and driving a 3 LED string.
When the input voltage dips below the required operating voltage of the LED string, the device, as expected, starts to operate at 100% duty cycle and the LED current drops below the set point.
However, when the voltage then rises above the required LED string voltage and the current exceeds the set point value, the drive to the LED's remains on and the current rises well above the set point.
The device continues to operate at 100% duty cycle even though the current limit is exceeded and does not recover for up to 4mS once the input voltage is high enough.
Any ideas as to why the drive to the LED's does not switch off?