Hi,
Does it possible for controlling multiple LEDs with one engine in LP5562? Because I want to achive the LED pattern like the attached files. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jerry,
With the LED PWM output selection bvits you can select which Engine controls which output. These bits are located in the register 70h (W_ENG_SEL, R_ENG_SEL, G_ENG_SEL and B_ENG_SEL bits). So all of the four LED ouputs can be controlled from one engine.
Thank you,
Sami
Hi Jerry,
Unfortunately there is not similar control as LP5523 row control.
To achieve the wanted sequence, you would need to use the triggering between engines, but then you can control only three LEDs independently.
Thank you,
Sami
Hi Jerry,
For that application it seems to be better solution. You can also check LP8501, which is close to LP5523.
Thank you,
SamI