Hi Everyone!
I need an information about TLC5917.
Please reply following question.
((Question 1))
Which type of sink driver about OUT0-7?
FET type or Bipoler Tr type?
((Question 2))
If Vdd(5V) power down but V_LED(9V) power on,
in this case, OUT0-7 sink driver is Stay ON or OFF?
((Question 3))
Is the SDI Input Pin broken when Vdd(5V) goes 0V and SDI Input is stay High(5V) input ?
((Question 4))
Is there EVM Design data(thermal design area) and observed real ψjt value ?
Best Regards
Shing