1. How many TLC5947 can be cascaded with the scanning mode of 1/16 and the spi frequency is 8 MHz , when the numbers are increased i will get the flickering effect in the display.
2. also give the explanation about the max INPUT FREQUENCY OF THE TLC5947 when cascaded.