I build a board with a LM3434, similar to the eval-board.
It should drive 1 LED with max 30A.
The switching frequency is 600kHz.
The driver works for about 30us then it stops and start again with a frequency of 10kHz.
The device is enabled and no dimming is active.
I make some modifications to the eval-board and this is running with 30A.
I need some hints what could be wrong and where to look.